Successful hunting exhibits in Dortmund and Salzburg

Stay flexible with the PUSH & GO multi-adapter

Whether used for hunting or sports marksmanship – the PUSH & GO sling swivel made by Erwin Halder KG has proven its worth time and again and is receiving tremendous praise from the marksmen community. No wonder seeing as the ball lock pin technology of the PUSH & GO sling swivel makes it possible to quickly and easily remove the rifle sling with the press of a button – and with no rattling or noise to boot.

“Kicking off the year with attending the hunting and fishing fairs “Jagd & Hund” and “Hohe Jagd & Fischerei”, we were finally able to taste trade show air again and meet the marksmen community face to face.  Trade show visitors in both Dortmund and Salzburg showed great interest in our PUSH & GO sling swivels as well as in the forest tools we selected to showcase at these fairs this time around“, rejoices Bernd Janner, Sales Director at Erwin Halder KG. “It is astounding to witness the high profile our products have now gained in the industry. Better yet, not only are many people familiar with our products, they are also highly satisfied with them, earning us positive feedback all around. We are delighted that those in attendance took advantage of the opportunity to receive a personal consultation and explore our product range in person.”

Halder announced that the big seller at this year's hunting fairs was the extremely versatile PUSH & GO multi-adapter. This adapter makes it possible to easily attach up to three Picatinny rails with hexagon socket screws in order to, for instance, mount a bipod with great speed and repeatability. Moreover, it features two integrated sockets for attaching a PUSH & GO sling swivel and a stud adapter. The lateral swivel range of the multi-adapter lets users effortlessly level out unevenness of up to 30° in the subsurface on which they place their firearm. The multi-adapter is made from lightweight materials – the combi socket from titanium and the adapter body from aluminium. These materials make the accessory exceptionally light.

At the heart of both the PUSH & GO sling swivels and the multi-adapter is the tried-and-tested ball lock pin technology developed by Erwin Halder KG. Attaching these little helpers to the rifle is lightning fast and perfectly noiseless. A push of the press button is all it takes to release them. The balls engage automatically in the locating bore when the button is released and are unlocked again with a press of the button. The matching locating bushings are fitted flat into the gun stock and can be retrofitted with no effort.

Halder’s extensive product range lets every marksman find the PUSH & GO sling swivel that is right for their specific use case: Depending on the model, they come in the standard diameters of 9.5 and 6 mm for sling widths of 23 and 40 mm. The sling swivels are available with a clamp collar for a shotgun barrel, as an upgrade kit for the Blaser bolt action rifles R93 and R8, and as a version designed especially for sporting rifles. In addition, Halder offers sockets for lateral attachment on the rear shaft and sockets with integrated swivels.

The sturdy PUSH & GO sling swivels and the locating bushings are made of stainless steel and have been treated with a black anti-corrosive coating. All models are, of course, suitable for outdoor use.

 

Messestand

Removing the sling swivel with speed and ease – trade fair visitors in Dortmund and Salzburg were given an opportunity to experience the supreme quality of the PUSH & GO sling swivels by Erwin Halder KG first hand.

 

Downloads: