Non-rebound, wear-resistant and gentle on the joints. As a specialist for corners and edges, the SECURAL soft-face mallet is perfectly equipped for laying parquet and laminate flooring.
Whether you work as an upholsterer or a saddler, you will find that the Halder soft-face mallet is tailored perfectly to your requirements. Better yet, a large selection of inserts, housings and handle types allows you to quickly customise your Halder hammer to your specific application needs.
When the going gets tough, only the tough get going? Au contraire! Especially the gardening and landscaping segment has a need for hammers with soft inserts as well. One example is the installation of slabs or tiles. This is why Halder offers soft-face mallet solutions that match all types of necessary applications - from extra hard to particularly gentle.
Whether your job at the workshop requires you to strike with all your might or to proceed with great caution, Halder is sure to have the soft-face mallet that is right for any type of assignment. To find the best match for your specific application, you can choose from an extensive assortment of inserts that vary in hardness and from a variety of housings and handles.
From brute force to exactly-dosed strikes to ultimate intricacy - joiner's work calls for hammers that cover a wide range of different jobs. And, these jobs can be mastered best with soft-face mallets from Halder as they can be fitted individually to match each specific application.
We all know that glass and hammers are natural enemies. That is, of course, unless you work with soft-face mallets from Halder. They have been specially designed to meet the requirements of the glazing and window construction trade. Aside from handling materials and workpieces with care, they are gentle on your joints and keep you from becoming fatigued. And, just like that, glass and hammers are the best of friends!
When you are working on the roof, the last thing you want to is scramble for the right tool. You want tools handy that let you work in a way that is safe, precise and as gentle on your joints as possible. In other words: tools such as the soft-face mallets from Halder, which are specially designed to meet the requirements of carpenters and roofers. To sum it up: no experiments!
Work on sheet metal and plumbing calls for an exceptionally delicate touch and controlled dosing of the applied impact force. And, when it comes to that, no hammer is like the other. This is why Halder offers a comprehensive selection of soft-face mallet models, all customisable to your individual needs. You can match your application with the right mallet by choosing from inserts with different levels of hardness and from different types of handles.
Whether hammers in metalworking are struck with great force or in well-controlled doses, the key is to keep the workpieces from becoming damaged. Carrying a wide selection of soft-face mallets and inserts, Halder can supply the right hammer for all kinds of metalworking applications. And, each hammer is guaranteed to be easy on both the material and your joints.
When work is piling up in the forest or on the farm, you need a tool that can clear away serious amounts in a short time while allowing you to work in a way that is non-tiring and easy on your body. Whether you need sledge hammers, splitting axes, hand axes, forestry sledges or tapers - Halder carries a comprehensive range of gentle striking tools for use in agriculture and forestry. They make your job easier - and take a load off your shoulders.
You as a floor layer will welcome anything that makes your job easier. This is why we at Halder design soft-face mallets - such as our SECURAL - that meet the specific requirements of each and every trade perfectly.
Working in upholstery and in the saddler's trade is full of different challenges - ranging from the gentle stripping of upholstered furniture to punching holes with great force. Good to know that Halder has the right hammer for all of your applications!
The requirements in gardening and landscaping are demanding and manifold. Conditions are often rough and difficult. You will thus need a tool that is perfectly dependable at all times. Our soft-face mallets have been engineered precisely for these types of jobs. Robust, reliable, and adaptable. Exactly the attributes true originals need to display every day.
Maintenance and repair work can take vastly different shapes. With the right pick of a Halder soft-face mallet you will be able to master all types of challenges - from assembling or disassembling gearboxes and engine blocks to changing wheels to such light work as the gentle loosening of plastic panelling.
One hammer to do it all? There is no such thing. At least not if you take your job seriously. This is because there is a clear difference between a task requiring a great deal of force, such as detaching an old door jamb, and a job involving delicate taps, such as work on a valuable piece of furniture. For this reason, Halder carries a wide variety of soft-face mallets, which share the option of precise customisation for all types of joiner's work.
Whether you use them during glazing or while installing windows and glass doors, the soft-face mallets made by Halder ensure that you will not break anything or leave behind blemishes.
Whether your work involves placing a roof truss, positioning beams or securing vapour barriers, you will find the tool to match each of your applications in our comprehensive product range. At Halder, you will everything that makes your work life easier: from the SIMPLEX soft-face mallet to the SIMPLEX sledge hammer to magnetic holders.
It clearly makes a different whether you must proceed with caution during crimping applications or need to apply sound strikes on piping. At Halder, you will find the right hammer in exactly the configuration that you need for your particular application - from the small BASEPLEX to the FERROPLEX combi hammer. Manufactured with premium quality and gentle both on your joints and your workpiece.
Positioning workpieces, loosening flanges, adjusting pipelines, aligning frames, opening moulds - the applications in the metalworking industry are just as varied as the soft-face mallets made by Halder. The name of our soft-face mallets are SIMPLEX, SUPERCRAFT or SECURAL, and you can customise their configuration to your specific needs.
Driving in stakes, splitting coniferous wood, hardwood, metre logs or kindling, wedging wood open, and inspecting trees - the jobs in agriculture and forestry are manifold and often demanding. Good thing to have a supplier in Halder who has the right tool for all of these jobs. Distinguished by its premium workmanship and abundance of model versions, it allows you to work without fatiguing and with minimum strain on your joints.