Eye bolts and other carrying elements have to be screwed in in a time-consuming way. Threaded lifting pins, on the other hand, can be inserted into existing threads at the push of a button and thus save an enormous amount of time when handling a wide variety of loads.

Threaded lifting pins are used when there are threaded holes with a counterbore according to DIN 332.