Easily clamp workpieces to the complete machine table with the sub-part clamp
10/06/2015
Clamp workpieces to the entire machine table and save space, if possible without interfering contours for precise and fast machining. Not exclusively, but for larger components in particular, clamping solutions which meet these requirements are a step towards even more efficient production. Erwin Halder KG from Achstetten-Bronnen, standard part manufacturer and expert for workpiece clamping, developed its new clamping device team, consisting of a sub-part clamp and stop, precisely for such applications. It addition, it can be adjusted easily to diverse workpieces.